You are here: Advanced Topics > Motion Techniques > PLCopen Homing > Homing Description

PLCopen Homing Description

The homing features provided in PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML create tools for homing of PLCopen axes. HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position may be performed utilizing the MC_Reference function block, utilizing Custom Homing Library UDFB"User Defined Function Block" UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB’s or by writing your own homing cycles.

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™